Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any way to make a linear pattern ?

Pioneer
Pioneer

I would like to draw along the same line with same distance and then cut out the shape. I dont wanna copy paste one by one.

9 REPLIES

Re: Is there any way to make a linear pattern ?

Gears Phenom Gears Phenom
Gears Phenom

Retangular pattern with one of the axis by 1 should do it or a pattern along curve...  and use a straight line as the curve...

 

???

 

seems to easy?  is that all that you are asking or am i missing your intent? 

 

can you show an image of what your desired output is?

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Is there any way to make a linear pattern ?

Pioneer
Pioneer

I didn't know how to use but I understood know. I used rectangular pattern. thanks

Re: Is there any way to make a linear pattern ?

Gears Phenom Gears Phenom
Gears Phenom

@Aeroeng  ok yes,  this is basic patterning..  nothing special...

 

Take a look at the SE HELP:   https://docs.plm.automation.siemens.com/tdoc/se/109/se_help#uid:featb3a

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Is there any way to make a linear pattern ?

Phenom
Phenom

Hi @Johnson_BigMatt

 

the patterning in SE is the most annoying command I met ( Ordered Environment ) and not easy to learn and understand.

I am not using this commmand often, maybe a few times a year and every time I have to dig for information to remember how to use it.

 

Tricky one,

 

cheers,

Arek


Production: SE ST10 MP8
;

Re: Is there any way to make a linear pattern ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @arekkul

 

 

maybe it is hard to learn by Yourself but if understand it once, I think You will see the rich possiblities of SE patterning.

Even in orderd mode

 

If You once have seen what fixed, fill and fit pattern will do for You, how easy and wonderful the Stagger option will work for You, You not longer will see pattern as something strange and bad, I think it will be the oposite.

 

But again, this is my private, personal opinion with less knowledge about other software packages and about their capabilies.

 

I only have heard, the last time two days ago, how complex and complicated it will be to get something like a fill pattern in other products at the market.

 



regards
Wolfgang

Re: Is there any way to make a linear pattern ?

Phenom
Phenom

Hi @hawcad

 

yes, you have right.

The Training makes you the master.

 

regards,

Arek


Production: SE ST10 MP8
;

Re: Is there any way to make a linear pattern ?

Honored Contributor
Honored Contributor

I have big problems with the pattern command.

 

#1 you cant change the pattern after it has been created

#2 the process to create is long, and since no editing can happen afterwods, you have to get through the entire process without any mis-clicks.

 

I bring this up because I could be missing something or a way to edit the pattern later.

Re: Is there any way to make a linear pattern ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You certainly can change the pattern later.

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Is there any way to make a linear pattern ?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @12GAGE

 

 

changing everything from a pattern is easy to achieve.

 

You either can go to the variable table and change the pattern parameters, as long as the change will be a numerical one only.

 

Or You go to the pattern feature into the Profile environment, select the pattern sketch (rectangle or circle) 

what will offer You the full possibilities of pattern options and settings.

 

 



regards
Wolfgang