Cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with bend lines disappearing after modifying the flat

Phenom
Phenom

I keep having an issue, usually on rolled parts, where when I modify the flat pattern it results in the bend lines disappearing in the draft. I would understand if I had made a tabe that crossed the bend, but I haven't. Just added material to the ends. What can I do to remedy this?

(view in My Videos)

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
4 REPLIES

Re: Issue with bend lines disappearing after modifying the flat

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @nominus38,

 

Yeah, this can "sometimes" happen, when the material that is added, consumes the entire edge of the bend.

In this example, I presume the part is actually formed from a longer blank, then run-off's trimmed away, as is why you're adding them in the "Flatten" model.

 

Can you afford to have "very small" straight segments on the ends your finished part model?.....I think this would then work as expected.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Issue with bend lines disappearing after modifying the flat

Phenom
Phenom

I have already done what you have suggested, but I hate it. Since you say that it's when it consumes the entire edge, does that mean if my tab say didn't run the whole length of that edge would it still show the bend line? If so I could always just draw the tab with a very tiny relief so it doesn't run that full length.

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Issue with bend lines disappearing after modifying the flat

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Correct.....just tested it here, and it works.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Issue with bend lines disappearing after modifying the flat

Phenom
Phenom

Awesome. Thanks.

ST9
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"