Cancel
Showing results for 
Search instead for 
Did you mean: 

Issues with SE renaming files in STEP conversion?

Creator
Creator

When I attempt to convert a STEP file to asm, I lose a portion of the names associated with the respective parts inside of it. From what I can tell, everything after the underscore is removed in translation. Is there a default somewhere I can change to fix this, such that I get the full part names in translation? I'm attaching what my coworker opens in Autodesk versus what I get when I use SE to show the issue. 

STEP_InorrectNames.JPGSTEP_CorrectNames.jpg

1 REPLY 1

Re: Issues with SE renaming files in STEP conversion?

Gears Phenom Gears Phenom
Gears Phenom

can you confirm that the origianl file name is the OS name and not a property or concatination of multiple properties.

 

this is my guess,  waht is displayed in not really the File name but rather a property or multiple properties so the translation is only handeling the FIle name as Step does not read properties / attributes.

 


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7