Cancel
Showing results for 
Search instead for 
Did you mean: 

It will stitch but won't turn into a solid

Valued Contributor
Valued Contributor

Once again, I am trying to turn a stitched surface model into a solid, but it won't do it. I have no errors when I inspect the model, don't see any unstitched or overlapping edges. Anyone have any workarounds to get it to turn into a solid? Happy to attach the file or send it to you if you want to take a look

Regards

Peter Smith

7 REPLIES 7

Re: It will stitch but won't turn into a solid

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Can you right click on your stitched surface feature and select Make Base Feature?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: It will stitch but won't turn into a solid

Valued Contributor
Valued Contributor

No, that is greyed out.

Re: It will stitch but won't turn into a solid

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Going to have to share it then.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: It will stitch but won't turn into a solid

Valued Contributor
Valued Contributor

Here is a dumbed down version of it.

Re: It will stitch but won't turn into a solid

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

There are two small "opened corners" on your model.

 

I've attached a dumb file, but it is a body.

 

Here is a video about steps (sorry for HUN UI):

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: It will stitch but won't turn into a solid

Valued Contributor
Valued Contributor

Thanks! I was looking in the wrong spots for the open corners!

HUGE help.

Regards

Peter 

Re: It will stitch but won't turn into a solid

Valued Contributor
Valued Contributor
Ok...I did the same as you, stitched it all together and don't get a solid....GRRR...I am going to try using your parasolid file. Thanks for the help