Cancel
Showing results for 
Search instead for 
Did you mean: 

Jogs in coordinate dimensions prevent reattachment

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

I found a bug when trying to reattach a coordinate dimension that has a jog in it. Note that the jog was created pre auto-jog features in SE but it still shouldn't have an issue.  

 

1.  I deleted a hole in the part and created another one at a new location.

2.  I updated the view and the dimensions became detached as expected

3.  I reattached the X axis coordinate dimension to the new location with no problem

4.  The Y axis coordinate dimension will not show the grab point for the dimension - the dotted gray line is there, but nothing to grab

5.  I remove the jog and now the grab point appears and I can now reattach the dimension.

 

Here is a Jing video

 

http://screencast.com/t/NPjmkzSRjua

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
1 REPLY

Re: Jogs in coordinate dimensions prevent reattachment

PLM World Member Legend PLM World Member Legend
PLM World Member Legend

Yes this been a problem for awihile. but, if you use "Attach Dimension" it works fine. Thats all i use