Cancel
Showing results for 
Search instead for 
Did you mean: 

KeyShot Nurbs

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

 

I'm having a problem where rounded faces or edges appear faceted, so I want to use the NURBS mode to smooth those edges or faces. But I cannot use it as it appears gray.

 

Can anyone explain me how to use this mode or another way to smooth properly?

 

The file I'm using is from Solid Edge ST9

 

thanks!!!

2 REPLIES

Re: KeyShot Nurbs

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@gic_nx  I believe the KeyShot Nurbs option along with a few others (HDRI editor) is only available in KeyShot Pro or above which is why it is not activated in KeyShot CAD/HD.  You would have to upgrade your KeyShot license through the KeyShot.com site to get that feature.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: KeyShot Nurbs

Phenom
Phenom

@gic_nx Have you tried using the sharpen button on the View tab before exporting to Keyshot?

 

The sharpen function decreases the polygon (facet) size for rendering which makes it more detailed. I think, though I'm not sure, that this is then what gets exported to Keyshot. Hence if you sharpen your graphics view before exporting, the resulting render will hopefully be smoother.