Cancel
Showing results for 
Search instead for 
Did you mean: 

KeyShot and result of a stress analysis.

Genius
Genius

Hello Edger's,

 

Is in SE and KeyShot there are any possibility to make reneder witch stress analysis result without using third softwear's ?

SE ST9 + TC 10.1.7
2 REPLIES 2

Re: KeyShot and result of a stress analysis.

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Unfortunately, there is no way... Pls, ask an ER.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: KeyShot and result of a stress analysis.

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This is not a question to the OP, but why is this post pinned to the top ?