Cancel
Showing results for 
Search instead for 
Did you mean: 

Keyshot - Different paint on same beam

Hello,

I would like to make 3 different colours on the same beam.

For example see the below screenshot.

1005358 - SB 303 UMB - ER-200 B.167_1280pix.png

 

The vertical beam has RAL 9016,RAL 5015 and RAL 3000. It is a client demand so I have to make this.

 

Who can help me to create this?

-------
Daniël Schuiling
3 REPLIES 3

Re: Keyshot - Different paint on same beam

Phenom
Phenom

You need to give a color in SE on each different face, than keyshot takes this over and you can change the color face per face.

...........................................................................................................
Solid Edge 2020 & AutoCAD 2020 user

Re: Keyshot - Different paint on same beam

That is what I thought, I only hoped that Keyshot was a little bit smarter for place a section coating on a beam.

Thanks Joris
-------
Daniël Schuiling

Re: Keyshot - Different paint on same beam

Worked, see the quick and dirty screenshot.

untitled.170.jpg

I did it with split Smiley Happy

-------
Daniël Schuiling