Cancel
Showing results for 
Search instead for 
Did you mean: 

Keyshot: How to refresh?

Valued Contributor
Valued Contributor

Hi,

 

I have saved an old Keyshot with rendering details etc. of an Assembly of mine.

When I open it, then it contain an old version of the assembly, not the newest one.

 

Do you guys know if it's possible to "refresh" the assembly in Keyshot, so I update to receive the newest version of the file?

 

 

 

Regards,

 

Kenneth

6 REPLIES

Re: Keyshot: How to refresh?

Phenom
Phenom

Kenneth,

 

You may need to have the Assembly in Solid Edge open, then click on Keyshot Update in the Solid Edge Tools menu.

 

Not sure this will work, but it's worth a try. If not tray opening both programs and see if that will work.

 

Bob

Re: Keyshot: How to refresh?

Legend
Legend

Bob is on the right track: You open the assembly in SolidEdge, open Keyshot from SolidEdge, and Keyshot will confirm that you have already saved this, and it will then update.

ST8 MP9
Go FAST, or go home.

Re: Keyshot: How to refresh?

Valued Contributor
Valued Contributor

I have tried this but it does not work.

My old render is saved at BIP (can't check if the name is correct atm.) and it does not update when I open it, even when I have both programs open etc.

 

I will post an video of it when I get home.

Re: Keyshot: How to refresh?

Legend
Legend

I'm new to using Keyshot with ST7, and my saved .bip stuff updates if I open with SE first.

ST8 MP9
Go FAST, or go home.

Re: Keyshot: How to refresh?

Valued Contributor
Valued Contributor

What if you save a new bip, close both Keyshop and SE. Then open SE and the old bip (with old version if assembly), will the bip still update for you?

Re: Keyshot: How to refresh?

Gears Phenom Gears Phenom
Gears Phenom

The bip reads the Solid Edge geometry and the file name too but does not retain a link to the path of the Solid Edge part. The .bip file when viewed in WordPad reveals this.

 

anchorwire.png

 

The name of the Solid Edge document is used to create some groups and stuff but after this Keyshot copies all vertices of the traigulated (tessellated) SE object and stores locally:

 

anchorwire2.png

 

So chances of any linking and updating of changes made to the SE model are less, unless there are is such explicit functionality provided by Keyshot, other than the Update button in SE. Just my interpretation.

 

As for your last question - yes, it is just the Update button away if both the new SE model and the old bip are open.

 

But your original question - ideally that should be the case.

 

~Tushar