Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Keyshot fun

Phenom
Phenom

@spindler wrote:

My first Projekt


@spindler  Whoa, I didn't know you could do things like that with the light and the shadowing and all. I really gotta get some time and learn keyshot. I wanna be able to do that.

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Keyshot fun

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@nominus38, yeah my thought also.......really neat animation @spindler

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Keyshot fun

Gears Phenom Gears Phenom
Gears Phenom

We use keyshot to show our chairs. We don't make real artwork of our renders like I see here, but I am very happy with the result after just 10 minutes of work.

key767.80.jpgzitting.82.jpg

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: Keyshot fun

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

http://www.acam.at

Re: Keyshot fun

Creator
Creator

I'm kind of new to the Solid Edge / Keyshot game but I LIKE IT!

 

Here are two kitchen things which worked out pretty well

Downdraft-Linear-Closed.JPGDowndraft-Linear-X.JPG

Re: Keyshot fun

Community Manager Community Manager
Community Manager

Nice! The use of focus/out of focus makes it so real. Great job.

Dan Staples
Director, Solid Edge Product Development

Re: Keyshot fun

Phenom
Phenom

@JoJoNL, you call that "pretty well"? Pretty **bleep** awesome more like.

Re: Keyshot fun

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Solid Edge 2019 comes with Keyshot7...

 

KS1068911081.20.jpgKS1068911081.15.jpgKS1068911081.2.jpg

Highlighted

Re: Keyshot fun

Gears Legend Gears Legend
Gears Legend

Hello Keyshot and Visualisation Fans,

 

Have found a very nice function in Windows 10 Build 17134.112

With this, you can easy animate pictures and create short clips.

Open a picture (create with Keyshot as example) with the integrated photo view from Windows 10 and then click on create animation (3D effect) or create a clip and then on animation (3D effect). It is now more a beta version but I hope it will grow fast with more and better effects too. Here are some example I have create with the tool very fast.

(view in My Videos)

 

(view in My Videos)

 

Best Regards

Wolfgang

Re: Keyshot fun

Phenom
Phenom

I love the guy welding in the second video... nice job!

 

Bob