Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Keyshot fun

Legend
Legend

Hello @BobMileti,

thank you for liking it.

This is a simple template from 3D Animation in Windows 10 (please forgive me in English) called "lightning". The steam is “breath” and so on. It is very simple to use. But I hope in the next versions it grow a bit more to get some other animation templates. Also I hope it will be allowed to work with levels and shapes.

 

Best Regards

Wolfgang

Re: Keyshot fun

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

I started modeling from scratch when the World Cup football final 2018 Croatia Vs. France started, with the goal to finish the assembly during the match.

Had the match run into extra time, the quality of renderings would have been much better Smiley Wink

 

So here are the snaps when the trophy was being awarded to France.

 

FoosBallSE_01.png

 

FoosBallSE_02.png

 

FoosBallSE_03.png

Re: Keyshot fun

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Tushar

 

 

well done - a great job!

And just in time (good time)

 

Smiley Happy

 

regards
Wolfgang

Re: Keyshot fun

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Thanks Wolfgang.

I think I should have started a bit earlier during the tournament to get better results of rendering Smiley Happy

 

Regards,

Tushar

Re: Keyshot fun

Experimenter
Experimenter

It's awesome, both rendering and the victory of th France Smiley Tongue

Highlighted

Re: Keyshot fun

Gears Phenom Gears Phenom
Gears Phenom

A bit of fun using Solid Edge 2019 Academic plus Keyshot 7.

Mobius Band.

Enjoy!

 

KS®20254127.1.jpg

Regards,

Arek

 

Re: Keyshot fun

Gears Phenom Gears Phenom
Gears Phenom

Another item made by using Solid Edge 2019 Academic.

Big thanks to Nishant Gautam

 

KS®852812674.3.jpgKS®852812674.2.jpg

 

Re: Keyshot fun

Gears Phenom Gears Phenom
Gears Phenom

This has nothig to do with keyshot but there's nowehere else to really post it. Some of you may have already seen this image in Siemens marketing. This photo, of one my customer, was taken by a photographer friend of mine, Quick overlay in Solidedge to (try) recreate  the same perspective. Then edited using a phone app actually Lol. Came out pretty decent. I'd like to get the model orientation a little better and then have someon with real photo editing blend them together.

Click on attached file link at bottom of post to see larger image!

 

OVERLAY_small logo (small).jpg

 

 

 

 

 

 

 

-Craig

Re: Keyshot fun

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This image is beyond awesome - gives me a rush every time I see it.

Re: Keyshot fun

Gears Phenom Gears Phenom
Gears Phenom

Here's the two original photos

 

17score-baja500-herbst-40.jpg01-smaller.jpg

-Craig