Cancel
Showing results for 
Search instead for 
Did you mean: 

Keyshot is broken

Legend
Legend

Hello,

 

I updated Keyshot to the newest version. For some reason the update failed in the middle and I had to abort the update. Now when I try to open Keyshot inside Solid Edge or stand-alone, I get the following error message:

 

"This application has failed to start because Qt5Core.dll was not found. Re-installing the application may fix this problem."

 

Is there any way to fix this issue without having to re-install Solid Edge completely?

3 REPLIES

Re: Keyshot is broken

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Have you tried "repair" instead of "uninstall"?

Bruce Shand
ST10 MP7 - Insight - Win10 - K4200

Re: Keyshot is broken

Community Manager Community Manager
Community Manager

@Teemu We reproduced this here in Huntsville and will notify Keyshot.

Laura

 

Re: Keyshot is broken

Community Manager Community Manager
Community Manager

@Teemu

Also - we reran the Keyshot update installer WITH SOLID EDGE CLOSED and the Keyshot update worked fine.

 

You should not have to remove Solid Edge.

 

Laura