01-14-2016
07:35 AM
- last edited
Monday
by
AmyReyes
01-14-2016 02:36 PM - edited 01-14-2016 02:37 PM
Hi there @TRC,
I'm at work, using the commercial version, so can't open your file....but, do you want to have a physical model of the knurling?,...or are you OK with a texture, like Solid Edge uses for threads??
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000
01-14-2016 03:00 PM
Yes, that would be fine. Thanks for your help.
01-14-2016 03:51 PM - edited 01-16-2016 12:35 AM
OK...[recycling the model from your thread question here ] for applying a texture, go to Style on the Home tab, select Face Styles, I preselected the thread, and chose "New", making a Knurling [Square] entry, then on the Modify Face Style dialogue, I went to the Texture tab, and applied the image I had saved [see attached texture image "Knurl-1"] in the Solid Edge textures location. [check the Help file for more detail on this]....can also use "Part Painter", with selection method set to "Face" to apply this texture.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000
01-14-2016 04:02 PM
Thank you very much for all of your help.
TRC
01-14-2016 04:10 PM
Very welcome!
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000