Cancel
Showing results for 
Search instead for 
Did you mean: 

Language of Standard Parts

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

 

Before delating de register of Standard Parts all of these menus are in spanish. Captura.PNG

I try to restore the registry but it does not change.

 

 

How can I change the language of Standard Parts?

 

3 REPLIES 3

Re: Language of Standard Parts

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Open registry editor!

Go to Computer\HKEY_CURRENT_USER\Software\Unigraphics Solutions\Standard Parts\Version 110 & here you will see the following registry key: "RuntimeLanguage", double click on it and edit its value from 1034 to 1033 in decimal mode.

 

Try to open STP Administrator!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Language of Standard Parts

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi @Imics,

 

Thanks for your reply but it don't change the lenguatge.

 

 

What do the registry numbers mean?

 

 

Xènia.

Re: Language of Standard Parts

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I just tested that language of ST10 Standard Parts is also dependent on ST10 language.

For example: If I use my local language (czech), I have Standard Parts in local language. If I switch language to english in SE Options - Helpers tab - Use english language, after ST10 is restarted Standard Parts are in english language.

I do not know if Standard Parts can be set to different language from SE as for ST9 or older versions.

 

Ota