Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Leg 3D

Pioneer
Pioneer

Good evening.

Through a real leg, how can I make a 3D through measurements? How should I proceed and what steps should I withdraw ?

 

Best regards,

Jorge Ferreira

18 REPLIES 18

Re: Leg 3D

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Your question is very vague. Too vague.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Leg 3D

Pioneer
Pioneer

What steps need to take a real leg, to do something in 3D. In other words , I want to make a piece to fit on one leg , but for that I have to create the object in 3D. How can I make a leg 3D only with specific measures ? Type , perimeters , widths , heights, etc.

Re: Leg 3D

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pakito,

 

Are you talking about 3D model of a human leg?.....maybe you could post a picture of what you have &/or need.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Leg 3D

Honored Contributor
Honored Contributor

I would go look for existing models that can be tweaked to a specific person. I know there are body models for a program called poser. I'm sure there are many starting file out there. The real trick is dealing with how it moves and changes. You will likly need 2 to 20 different states depending on required accuracy/flexibility

 

If you end up modeling from scratch, SE is not the best Nurbs package that is the most fitting control geometry to the human body and a simple computer model. Rhino would be a better fit to you're ends. Then export from Rhino to SE to make the "Add-on" to the existing leg.

 

Nurbs=non-uniform rational B spline. or a curve that fits point with specific ordered controls.

Re: Leg 3D

Pioneer
Pioneer

To make for example a soccer shin guard . What measures have to be of a human leg to make it fit in the leg ?Exemplo.jpg

Re: Leg 3D

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Pakito,

 

As they [Shin Guards] are a maluable item anyway, I wouldnt' get caught up in the intricate details of a limb.....just gather a few sectional type profiles at appropriate spacings to capture the "simplest form" you can, then recreate them into Solid Edge as sketches, surface loft those, trim to a boundary profile, and thicken the result to have a solid model of the part.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Leg 3D

Gears Phenom Gears Phenom
Gears Phenom

Are you going to make custom shin guards?

 

If so, you'll have to start with scanning the leg(s) and turning the point cloud data into usable mesh or surfaces.  You'll need a 3rd part app for that because it is not something that Solid Edge can currently do.

 

Once you have the surface, then you can bring it into Solid Edge and use it as construction geometry to reference when creating your actual parts.


____________________________________
--Scott Wertel, P.E.

Re: Leg 3D

Pioneer
Pioneer

I have a 3D scanner, but was wondering if the distance and through some points / leg measures could create a mold similar to the actual measurements . Measure the width of the leg, or perimeter , you can not make a mold?

Re: Leg 3D

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Pakito,

 

So do you have your scanned data already prepared and in Solid Edge?.....

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000