Cancel
Showing results for 
Search instead for 
Did you mean: 

Lic over internet

Experimenter
Experimenter

Is it possible to connect with a license server which is connected to internet, but not connected to your LAN (via internet connection only)? I think in that case we have to add the ip address of the license server along with host id. Can anyone help me doing so?

1 REPLY

Re: Lic over internet

Valued Contributor
Valued Contributor
I cannot answer your question directly however it seems ST9 will be good for you. There is the option to have the licensing cloud based. There is a good blog post on this site about it.

https://community.plm.automation.siemens.com/t5/Solid-Edge-Blog/Solid-Edge-ST9-and-the-Cloud/ba-p/34...

Another option is to borrow a license but this assumes a license can be obtained initially.


CAD/CAE Manager
ST8 MP9