Cancel
Showing results for 
Search instead for 
Did you mean: 

License Utility for ST10 does not start

Creator
Creator

Hello,

I've been searching the forum all day and couldn't find an answer to my issue

I've tried installing ST10 today( we have been using in the company the 2d free version) on a new machine.

After install I receive the "Your copy of solid edge must be licenced..." message and then nothing happens

What I have tried so far:

- reinstall (of course, reboot too)

- using the Licence Utility from start menu or install location

- changing the Licence Utility compatibility and rights

I have ran out of options at the moment

 

below is the sysinfo

 

Summary report (11/27/2017):

Solid Edge ST10 64-bit information:
FileVersion: 110.00.00.107
ProductVersion: 110.00.00.107 x64
Elapsed session time: 0:00:00:00
Internal session time: 0:00:00:02
Cumulative session time: 0:00:00:00
System information:
Sold-to ID:
Owner: General Electric
Company: General Electric
User: 502043503
Computer: Dell Inc., Precision 5520, x64-based PC
Operating System: Microsoft Windows 7 Professional Service Pack 1 64-bit (English) 6.1.7601
Processor information:
Intel(R) Core(TM) i7-6820HQ CPU @ 2.70GHz, GenuineIntel
Physical:1, Core:4, Logical:8, HT:Enabled, Clock:2.701Ghz
Global memory status (inuse/avail/total):
Physical: 3489MB/12430MB/15919MB, PageFile: 3730MB/20379MB/24109MB, Virtual: 156MB/8388451MB/8388607MB, Load: 21%
Process: 119.77MiB (committed), 52.64MiB (reserved), 8191.83GiB (free)
GDI objects: 159, USER objects: 4
Video adapter information:
Adapter: Intel Corporation, Intel(R) HD Graphics 530, 21.20.16.4664, Hybrid
ChipSet: Intel(R) HD Graphics Family, Internal, 72MB
Bios Info: Intel Video BIOS
GDI Driver: cdd.DLL (0.0.0.0)
ICD Driver: ig9icd64.dll.DLL (21.20.16.4664)
Topology: Homogeneous,DPIAware
Display: [1,1,1,0]Generic,1920x1080@60Hz,{v=120x120,p=140x141}dpi,125%,Intel(R) HD Graphics 530,Internal,Primary
Application information:
AppDisplay(Ac,Hx);RegionMode(Unset);Stereo(No);3DI(No);Effects(DC,MA,TF,MF);Scale(125%);
Culling(Yes,20%);DynTransition(Yes,50%);AutoSharp(High);Shaded(RP,HL);Glow(0);GAA(None,Pending High);GFR(100%);
Addin information:

 

15 REPLIES 15

Re: License Utility for ST10 does not start

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You could try to restore factory settings using the settings and preferences wizard.

Reinstalling does not clear the registry.

"C:\Program Files\Solid Edge ST10\Program\SECopySettingsWizard.exe"

LMGi
www.TLMGi.com

Re: License Utility for ST10 does not start

Creator
Creator

thanks, I've also tried that witout success

Re: License Utility for ST10 does not start

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

are you using the free2d version ?

if so try launch the program and use last option (see attached screen).

bye

 

Re: License Utility for ST10 does not start

Creator
Creator

Thank you tech-value, but I cannot get to that part. I'm trying to launch it and it just does nothing

Re: License Utility for ST10 does not start

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

- check system event viewer, maybe issue is related to a system component

- check AV logs, try to disable real-time protection during install

- if you have .NET framework 4.7 uninstall it, reboot and retry

- retry install in another path like   c:\Siemens\ST10

- cross your fingers Smiley Happy

Re: License Utility for ST10 does not start

Creator
Creator

I've tried the above, except net, which is older version, no more fingers to cross Smiley Very Happy

 

EV shows the below, for every launch:

Faulting application name: SELicWiz.exe, version: 110.0.0.107, time stamp: 0x597b3e26
Faulting module name: SELicWiz.exe, version: 110.0.0.107, time stamp: 0x597b3e26
Exception code: 0xc0000005
Fault offset: 0x00000000000725e2
Faulting process id: 0x2278
Faulting application start time: 0x01d3684bdd9356ae
Faulting application path: C:\Siemens\ST10\Program\SELicWiz.exe
Faulting module path: C:\Siemens\ST10\Program\SELicWiz.exe
Report Id: 1b57a47a-d43f-11e7-9e44-f894c20bcdf8

Re: License Utility for ST10 does not start

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @Ranton

 

 

just a couple of toughts.

 

  • You have sufficient rights on this computer
  • during installation, have You started it with "Run as Administrator"
  • and were the User Access Control turned OFF

 

regards
Wolfgang

Re: License Utility for ST10 does not start

Creator
Creator

Thanks for the reply @hawcad, I have tried your suggestions twice but nothing changed in the results

Re: License Utility for ST10 does not start

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Ranton  Have you tried having another user logon to the PC with a different account?



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com