Cancel
Showing results for 
Search instead for 
Did you mean: 

License problem

Experimenter
Experimenter

Hello,
I am having issues with ST6 on Windows 8.1. Solid Edge istalled without any errors but when i try to run it i get this popup.

Bez tytułu.jpg

when i click OK i get

Bez tytuł2u.png

then I go

Bez tytułu3.png

click OK and nothing happens.

 

I tried following some advices like: turning off antivir, edit someone elses license file etc. but nothing seems to be working.

Appreciate help,
Matthew

19 REPLIES

Re: License problem

Experimenter
Experimenter
Same error

Re: License problem

Experimenter
Experimenter

I havw same problem....

Re: License problem

Experimenter
Experimenter

Is there any way support could generate licence file for us? Even though licence manager seems to be working fine it does not create SELicence.dat file. This might be the soultion here.

Re: License problem

Experimenter
Experimenter

Yes, a friend used a License file and it worked well.

Re: License problem

Experimenter
Experimenter

Unfortunately my Examination time will start soon. feeling blue. 

 

So, I can't join the team to solve this problem now. 

 

Could you please upload how to solve with easy English and screen shots. 

 

My condition is follows 

  OS : Windows 8.1Pro 

  Installation file : SolidEdgeV106JAPANESE_32Bit 

   

 

Thank you in advance 

Re: License problem

Experimenter
Experimenter

I can't find SELicence.dat in my PC.

Could you please help?

Re: License problem

Experimenter
Experimenter

You can not find it because it is not there. The manager should generate one for you but it does not which is the source of whole problem. I thought support team is on this forum but it looks like we will have to contact them personally and ask for sending the file. 

P.S. the license file should be located in /Solid Edge ST6/Program/SELicense.dat

Re: License problem

Experimenter
Experimenter

I really would like to help you, but i don't know where he found the file.

 

I didn't do that on my computer, i'm waiting for support too.

Re: License problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Just to be sure here...as there are different methods for what type of install you are doing.....if this is indeed "Student Edition", then you will have been emailed the correct license file [or Code], with instructions on how to install it.

However, if you are installing and licensing the "Academic Version", then you will have to be provided with the code for that, which I think is provided directly from the school/college/university.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP7] Classic [x2 seats]
Windows 10 - Quadro P2000