Cancel
Showing results for 
Search instead for 
Did you mean: 

License

Experimenter
Experimenter

I have installed the free trial Solid Edge st7. When I try to open the application it says I need to register it first. When I type in my emil address it says that I am already registered. So I am going in circles. It seems I need a Webkey which I also cannot locate. Any suggestions?

4 REPLIES

Re: License

Siemens Phenom Siemens Phenom
Siemens Phenom

The license gets automatically applied when you install the software.

 

You do not need any webkey. This is for users who have purchased Solid Edge. Are you trying to run Solid Edge 2D Drafting through Remote Desktop? It will not run that way. You must be on the machine that the software is installed.

Regards,

Rick B.

Re: License

Experimenter
Experimenter

I am on the machine on which it is installed.

When I try to open the application I get the following:

Your copy of Solid Edge must be licensed for first-time use.

David

Re: License

Siemens Phenom Siemens Phenom
Siemens Phenom

David,

Sorry, This was posted to the 2D Drafting Community site so I did not pick up on it being the Solid Edge Free Trial. I'll get someone to reply.

Regards,

Rick B.

Re: License

Experimenter
Experimenter

Thank You.