Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Line width when printing

Valued Contributor
Valued Contributor

Hi folks I have a preblem here! Maybe someone can give me a hand...

 

First, check out the two attached pictures:

 

1) PrintViewerOn.png: Solid Edge Options => View => Display as printed on

2) PrintViewerOff.png: Solid Edge Options => View => Display as printed off

 

If i print the drawing (with updated drivers) I get a drawing with thick outlines as seen in picture 1). I would like to print as seen in picture 2. I tried all possible settings but could not get it right so that the outer lines would be 0.5mm thick and the hatched lines would be around 0.3mm thick.

 

Does anybody know how to accomplish this? I'm using Solid Edge ST8.

 

Thank you in advance

PL
8 REPLIES 8

Re: Line width when printing

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Under Solid Edge Options, View tab, is an option - Display as Printed.

See if changing this setting helps.

 

2016_Aug_04_01.png

Re: Line width when printing

Valued Contributor
Valued Contributor

Hi Tushar, thank you for your feedback.

 

The option you are describing is not the solution because I can only change my 2D view but not the actual printout paper line thickness. As you can see in my description I tried that already without success. Independantely of the option on/off the printout of the actual sheet is always with fat lines and not as it should look like (compare PrintViewOff.png).

 

Any other suggestion?

PL

Re: Line width when printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

All this depends on printers resolution capabilities and the printer driver's resolution setting (make sure your printer driver is set higher like 600 DPI or better).  The correct way to control the thickness is by specifiying the Solid Edge Line styles.  Keep in mind that if you print a drawing sheet at anything other than full scale, the line weights at the printer may be scaled.

 

We have our visible lines set to .2 mm and hidden lines set to .1 mm.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Line width when printing

Valued Contributor
Valued Contributor

Thank you for your answer Grundey

 

The printers resolution is higher then 600dpi (Epson R2880 5.760 x 1.440 dpi). My settings are set accordingly so this cannot be the problem.

 

Since your are writing; quote starts here:  "The correct way to control the thickness is by specifiying the Solid Edge Line styles" end of quote.

 

I already played around with the Line styles but could not get it done. I still had the fat lines when turning on Print View ON or printing a sheet. I will try to change the line style to 0.2 or 0.1 as you suggested and report the results...

PL

Re: Line width when printing

Valued Contributor
Valued Contributor

Grunday, your hint with the Styles helped. Smiley Happy

 

I could identify the hatched lines in the material section in the part environment (see pic below):

 

MaterialHatchPattern.PNG

 

In my case Normal Mesh was selected. Now that I knew what hatching style was set I could go into the drafting and selected View => Styles:

 

MenuStyle.PNG

 

Here I went into the menu and set the line width to 0,25mm.

 

LineSettingsHatchLine0_25mm.PNG

I could confirm the change that the hatched line in the drawing became more narrow i.e. 0.25mm. I then verified if this would also hold true when display as printed was set to on: Solid Edge Options => View => Display as printed set to ON (Checked). After checking display as printed to on the line remained with the correct width. Next, I printed the drawing to verify. After printing the drawing I measured the line thickness and could confirm that the width was correct.

 

VerifiedVisualLine0_5mm.JPG

PL

Re: Line width when printing

Pioneer
Pioneer

@PL, thanks for pointing the way to the line styles. I was expecting them to be located somewhere under Solid Edge Settings -> Options...

 

Unfortunately, in my SE 2019, despite turning off all paper and line scaling settings that I could find, selecting the correct paper size, and line style settings being as desired, on the printout I get 0.35mm lines where they should be 0.25mm, 0.7mm where they should be 0.5mm, etc. The same happens when I svae the drawings as pdf: all lines in the pdf are thicker than specified in the line styles.

 

Any idea what I am doing wrong?

Re: Line width when printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @DvG

 

 

 

there are options for printing to scale line witdh in reagrd with the paper size.

Maybe this is active.

 

 

regards
Wolfgang

Re: Line width when printing

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@DvG  There are a lot of variables in what you get on paper.  Your print driver may affect it, your print driver settings may affect it, the brand and quality of the printer may affect it, the print method may affect it (inkjet vs. laser), the paper may affect it, and the print feed direction may affect it.

 

I think the concept of line thicknesses is more about the width ratio between the printed line types rather than the actual width of the lines printed on paper.

 

I always recomend using the PCL version of a print driver when there are other versions available.  I would also make sure your print resolution is at least 600 DPI or better.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com