Cancel
Showing results for 
Search instead for 
Did you mean: 

List

Creator
Creator

Hi, newbie here.

I want to add a statement here that if the first string in any of the 3 myStrList is "Dog" then don't include that list, in this case 'myStrList2'.

 

 

Dim myStrList1 As String = "Cat,1,3"
Dim myStrList2 As String = "Dog,5,6"
Dim myStrList3 As String = "Duck,8,9"

Result = myStrList1 + "," + myStrList2 + "," + myStrList3

'The results = Cat,1,3,Dog,5,6,Duck,8,9

 

Thanks

Rulestream ETO Version 8.12.0.7556
Solid Edge ST7
2 REPLIES 2

Re: List

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi:

 

Just F.Y.I. there's dedicated Solid Edge Developer Forum where you can post coding related questions but I doubt this one. There's seemingly nothing in the query that is Solid Edge API related.

 

You can try posting this on a Visual Basic forum.

 

~Tushar

Betreff: List

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @JohnAsp

 

 

 

even if @Tushar is right in pointing to the developers formu I will try to answer here

 

 

I think it should be a combination of an IIF with an InStr like

 

Result = ""

 

for i=1 to NumberOfLists

  Result = Result & IIF(InStr(1, myStrList(ii), "Dog")>0,myStrList(ii),"")

next

 

 

 

Should work so

regards
Wolfgang