Cancel
Showing results for 
Search instead for 
Did you mean: 

Locked Dimensions, setting???

Builder
Builder

When creating a simple rectangle using the box command (pre-dimensioned), is it possible to have all the dimensions locked?

Rather than having to select each one and lock each one seperately!?!?

 

-Nate- 

3 REPLIES

Re: Locked Dimensions, setting???

PLM World Member Legend PLM World Member Legend
PLM World Member Legend
Using Auto-Dimensions for sketching (only when keyed in) does create driving dimensions. So, I looked at the IntelliSketch options for Auto-Dimensions, but that didn't seem to result in driving dimensions on the Box feature.

I am not an expert on Synchronous, so maybe someone else will know how to change that.

Jason

Re: Locked Dimensions, setting???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Don't believe you can as that goes against the direct edit philosophy of Synchronous.  Idea is you only lock those dims that have to stay static through all edits becuase it is critical to design intent.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com
Highlighted

Re: Locked Dimensions, setting???

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you expand the PMI section in the Path Finder(tree) you can click the padlocks without editing each dimension.(Fast!)

You can also Shift+Select a range of dimension and right click, lock many.

LMGi
www.TLMGi.com