Cancel
Showing results for 
Search instead for 
Did you mean: 

Locking a dimension in the Variable Table

Experimenter
Experimenter

Is there a way to lock a dimension controlled in the variable table, so that it can not be edited after publishing in Team Centre?

1 REPLY

Release it and then the whole file cannot be edited.  I d...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Release it and then the whole file cannot be edited.  I do not believe there is a way to lock a single variable from edit unless it can be done via custom code.



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com