Cancel
Showing results for 
Search instead for 
Did you mean: 

Locking a pattern in Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In Synchronous how do you lock a pattern dimension so it's not affected by a steering wheel drag? Can you? I think that calls for an ordered pattern, right?

Example: Say you have a simple rectangular plate on which you have a pattern of 4 holes. If I window one end of the rectangle and include 2 holes of the pattern the holes go with the edge when I stretch with the steering wheel.

Is there no way to lock the pattern?

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200
5 REPLIES 5

Re: Locking a pattern in Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you set the pattern to "Fixed", it will be locked.  If set to "Fill" it is not.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Locking a pattern in Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You're right, dangit! I tested the two settings before I posted and I thought they both behaved similarly. Now I did it and...

I must be losing it.

Thanks.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Locking a pattern in Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It was that extra day tacked on to the weekend... Smiley LOL



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Locking a pattern in Synchronous

Honored Contributor
Honored Contributor

I'm learning all kinds of stuff from your posts bshand.

Re: Locking a pattern in Synchronous

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Glad to hear it. You're not chopped liver yourself.

(I pity the international readers: "chopped liver"?!)

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200