Cancel
Showing results for 
Search instead for 
Did you mean: 

Loft command disabled

Creator
Creator

Hi

 

Im trying to do a loft cutout, but why is the loft command disabled?

-Thanks

 

R

7 REPLIES 7

What license type do you have?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What license type do you have?



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Hi there, This is because you have no material [protrus...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

This is because you have no material [protrusion] to perform the "cutout" to.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP8] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Highlighted

Re: Hi there, This is because you have no material [protrus...

Creator
Creator
Hi again

sorry, It is not a cutout but a protrusion I am trying to do.

R

Hi,   Maybe you have Solid Edge Design&Drafting license a...

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Maybe you have Solid Edge Design&Drafting license and it doesn't contain Lott functionality (and many others)...

 

BR,

Imics

Imics
http://solidedgest.wordpress.com/

Re: Hi,   Maybe you have Solid Edge Design&Drafting license a...

Creator
Creator
Hi again

My license is Solid Edge Classic and Design&Drafting, maybe thats why?

R

Re: Hi,   Maybe you have Solid Edge Design&Drafting license a...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Yes, it appears you are running the D&D license instead of the Classic.


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

ALL OF CUTOUT COMMANDS WILL BE INACTIVE TILL U HAVE A SOL...

Creator
Creator

ALL OF CUTOUT COMMANDS WILL BE INACTIVE TILL U HAVE A SOLID FROM WHICH U HAVE TO REMOVE SOME MATERIAL BY PURPORTING CUT OPERATION,.

 

BY PERFORMING CUT OPERATION, U R TRYING TO REMOVE MATERIAL. FACT -THERE IS NO MATERIAL IN THE PRESENT PART.

 

ASSUME WHAT U R DOING IS ACTUALLY TRYING TO REMOVE MATERIAL FROM A ZERO MM DIA ROD, AND U WANT 10 KG MATERIAL SHOULD BE REMOVED.