Cancel
Showing results for 
Search instead for 
Did you mean: 

Loft with Multiple non-continuous Guide Curves

Experimenter
Experimenter

Good day, I have recently migrated from Solidworks to Solid Edge and am facing some challenges related to Lofts in combination with multiple guide curves.

 

Due to the twist and change in profile as the body travels along the path I am forced to use guide curves, in a combination of edge locations.

 

Using this combination of profiles with either of the guide curves yields a successful loft, but when using them in combination it gives me the following error.

 

"All edges selected to be used as a path or cross section must be connected"

 

Have any of you faced this error before? Please advise,

 

Your help is greatly appreciated.

Capture.PNG

 

 

Mitch

2 REPLIES 2

Re: Loft with Multiple non-continuous Guide Curves

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You may be trying to pick both guide curves in one step where you need to pick one and accept it in order to progress the command so that you can pick the next one.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Loft with Multiple non-continuous Guide Curves

Experimenter
Experimenter

Thanks for the quick response! that resolved my issue.

 

MItch