Cancel
Showing results for 
Search instead for 
Did you mean: 

Lofted Sheet Metal from 3D sketch profile

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi Expert,

 

I have some issue here where I want to create a loft function in sheet metal using 3D sketch profile but failed.

 

Basically I want to use loft because I want to get the triangular line bend. (can refer my attachment)

 

For now what I do is by using surface and thicken it and blank it without the triangulation line. Is there anyone here able to do it?

Please refer my attachment.

15 REPLIES

Re: Lofted Sheet Metal from 3D sketch profile

Phenom
Phenom

First thing - I can't see any attachment.

I'm not sure if 3D sketches are permitted, but if they are I think they will still have to be planar sketches.

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Lofted Sheet Metal from 3D sketch profile

Solution Partner Builder Solution Partner Builder
Solution Partner Builder
Hi @beachcomber,

Thanks for the reply
My 3D sketch is not planar. refer the attachment.

Re: Lofted Sheet Metal from 3D sketch profile

Valued Contributor
Valued Contributor

Hi~ Arisy

do not know if I understand my explanation.
loft Flange does not support 3D sketching.

By the proposed method
1. Loft in a 2D sketch.
2. After that, cut it as shown in attached SM1 figure.

This is the only way.

Re: Lofted Sheet Metal from 3D sketch profile

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Arisy,

 

As others have mentioned, you are better off creating a "standard" lofted flange frome planar sketches first, then use "Normal Cutout" to get your desired final shape, that matches your 3D sketches.

 

SE_Transition_SR_Mod [Img-01].pngSE_Transition_SR_Mod [Img-02].png

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP1] Classic [x3 seats]
Windows 10 - Quadro P2000

Re: Lofted Sheet Metal from 3D sketch profile

Phenom
Phenom

@SeanCresswell

Nice Bat-Cape there Sean

HP Z420 16GB RAM
Quadro K4000
ST10 MP6 on Windows 10 Pro 64.

Re: Lofted Sheet Metal from 3D sketch profile

Legend
Legend

It would take a fancy press brake to form that in one piece!

Re: Lofted Sheet Metal from 3D sketch profile

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi

 

Thanks for the reply and suggestion. Now I have some idea.

Of course later on I will split this whole sheet metal into few pieces.

Re: Lofted Sheet Metal from 3D sketch profile

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi Sean.

 

Is there any faster way to calculate the length of the triangulation lines that I did here? Currently I need to calculate manually one by one by using DIstance between Dimension which need me to point starting point to the end point to measure.

 

Flat Pattern_BendLines.png

Re: Lofted Sheet Metal from 3D sketch profile

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there @Arisy,

 

I presume you are going to dimension this out for manual fabrication? [or do you need this for another reason, and in the 3D "Flatten" view??]

 

I would probably do that in the flat pattern view, from Draft, and just use Smart Dimension on the bend lines, laid out accordingly.

 

ST10_DFT__LoftedSheetmetal_FlatPattern_CreaseLength.PNG

 

ST10_DFT__LoftedSheetmetal_FlatPattern_CreaseLength-CloseUp.PNG

 

Hope that helps.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP1] Classic [x3 seats]
Windows 10 - Quadro P2000