Cancel
Showing results for 
Search instead for 
Did you mean: 

Lofted flange centered at assembly reference planes

Pioneer
Pioneer

How to place this two lofted flange with there outer bend radius against each other, centered at the reference planes of the assembly?

Find the part and assembly in the attachment.

Piket.jpg

2 REPLIES 2

Re: Lofted flange centered at assembly reference planes

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

Hello,

 

Is the tangency point of the bend radius on the reference plane?  If so, you can use the mate tool to place two occurances of the part.  You will probably also use mate to align the other planes because the planes are facing each other.

 

If the tangency point is not on the plane, use the tangent constraint tool to place the radii in contact with each other, then use the mate tool to align the other planes.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: Lofted flange centered at assembly reference planes

Pioneer
Pioneer

The tangency point is not on the plane. I tought the tangent relationship only worked between a radius and a face but is works also between radii.

I also found another solution. In the sheetmetal part I put a plane tangent to the radius and then related it with a mate to the reference planes of the assembly.

Thx.