Cancel
Showing results for 
Search instead for 
Did you mean: 

Logopress or simillar to SolidEdge

I see that there is an interesting application for SolidWorks, for progressive dies. It's Logopress. It exists anything to SolidEdge?

Tiago
6 REPLIES 6

Re: Logopress or simillar to SolidEdge

Gears Phenom Gears Phenom
Gears Phenom

Not familuar with the SW functionality but sounds maybe like EMBOSS?

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Logopress or simillar to SolidEdge

What's Emboss?

Tiago

Re: Logopress or simillar to SolidEdge

Gears Phenom Gears Phenom
Gears Phenom

https://docs.plm.automation.siemens.com/tdoc/se/109/se_help/#searchSmiley Tongueage=1;rpp=10;query=emboss

 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Logopress or simillar to SolidEdge

Gears Phenom Gears Phenom
Gears Phenom
forgive me for the confusion. I just ASS-u-MEd based on the name. "logo-press" sounded like a way to "press" a logo into a part.

So I goggled logopress and see that it appears there a 3 subsets of the tool: Tool and Die, nesting , & Blank

Blank is available in SE via either Sheet metal flat pattern or Blank Body command.
Nesting is available via some add ins. Sigma nest comes to mind : https://www.plm.automation.siemens.com/en_us/products/solid-edge/applications/manufacturing/sigmanes...


Tool and Die also via add-in:
see: http://www.summitsedge.com/training.htm
see: https://www.youtube.com/watch?v=Ip_1eddAyNA

see also https://www.plm.automation.siemens.com/en_us/products/solid-edge/overview/add_on_apps/mold_design.sh... not prog dia but...
Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7

Re: Logopress or simillar to SolidEdge

Honored Contributor
Honored Contributor

Sigma nest is one of the popular ones. Our parent company uses us and as a result, we plan to use it as well. An other one that is a step up is Radan, but it's also more $ but can tie into other systems better and is slick. Both are not cheap. The cost is tied to each destination for the files.

 

I believe there are cheaper ones out there, but they require tons more labor for each export. All of the nesting software costs more than the CAD software.

 

The EL-cheapo method is to export DXF, and arrange the DXF files on a sheet sketch and re-export.

Re: Logopress or simillar to SolidEdge

Phenom
Phenom

NX Progressive Die would be your alternative. Here you get the benefit of NX CAM and fefatue based machining, full associativity, etc. You also get FEA based solver for formability, thinning, etc.

Head to head NX will win.