Cancel
Showing results for 
Search instead for 
Did you mean: 

Low memory???

Experimenter
Experimenter

Could somebody, please, explain what's going on according to attached screenshot?

 

(SE ST6 x32 Academic Version on [Win7 x64 SP1 16GB RAM i7 3.4GHz] complains about lack of memory while there is plenty of that)

 

Thanks,

regards,

András

2 REPLIES

Re: Low memory???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hello András,

 

Your issue here is not Solid Edge, but simply a limitation of the 32bit application coding in >ST6....I suggest you upgrade to ST7 [is now 64bit only] to make full use of your great system specs.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: Low memory???

Experimenter
Experimenter

Thank you, Sean, ST7 works fine for what ST6 32bit simply crashed.