Cancel
Showing results for 
Search instead for 
Did you mean: 

Low performance issue in large Assembly

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

The customer is facing very low performance in large assemblies.The  assembly opening setting are according to large assemblies. any selected command will take 4-5 min for pop-up.

 

We tested on another machine with Quadro FX 580/600/610 card .

 

Show all component:20 min

This assembly is having 
UNIQUE PARTS= 3568
TOTAL PARTS= 15889
TOTAL SUBASM 1218
UNIQUE SUBASM 392

Plz recommned some good graphics cards .

18 REPLIES

Re: Low performance issue in large Assembly

Community Manager Community Manager
Community Manager

Something obviously unique going on. We have many customers with over 100K parts in assemblies and performance is nothing like this.A few things:

 

1. You need to state more about the configuration -- specifically which Solid Edge release and how much RAM on the machine?

2. Have you logged this problem with GTAC?

3. Was it working before? What has changed that suddenly caused this to occur?

 

 

Dan Staples
Director, Solid Edge Product Development

Re: Low performance issue in large Assembly

Community Manager Community Manager
Community Manager
PS> It is very unlikely anything to do with Graphics cards. This symptom is indicative of running out of memory (RAM). When you are out of RAM, all bets are off -- things that should take seconds take minutes.
Dan Staples
Director, Solid Edge Product Development

Re: Low performance issue in large Assembly

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter


Solid Edge 64-bit information (09/01/2015):
Version 107.00.08.05
System information:
Dell Inc., Precision WorkStation T3500
Microsoft Windows 7 Professional 64-bit (English) 6.1.7601
Processor info:
Intel(R) Xeon(R) CPU W3503 @ 2.40GHz
Physical:1, Core:1, Logical:2, HT:Cannot detect, Clock:2.40GHz
Global memory status (available/total):
Physical: 13718.15Mb/16381.55Mb, PageFile: 45816.77Mb/49147.74Mb, Virtual: 8388411.13Mb/8388607.88Mb, Load: 16%
Video adapter information:
Adapter: NVIDIA, Quadro K620/PCIe/SSE2, 9.18.13.4066
ChipSet: Quadro K620, Integrated RAMDAC, 2048MB
Display: 1680x1050x32 @ 59Hz
ActiveData: NVIDIA Corporation | NVIDIA Quadro K620/Quadro K620/PCIe/SSE2 | 09.18.13.4066 | WIN7 | HX | DX | DL,SL,MB
AutoConfig: NVIDIA | Quadro | * | WIN7 | HX | DX | DL,SL,MB
Validation: Solid Edge ST7 | Microsoft Windows 7 Professional 64-bit | NVIDIA Quadro K620 | Intel | 9.18.13.4066
ICD Driver: nvoglv64.DLL (09.18.13.4066) NVIDIA Corporation

Re: Low performance issue in large Assembly

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

The RAM is 16GB

 

This issue is already reported to GTAC a month ago. They are still working on this issue.
Siemens GTAC Support IR 7485666.

Re: Low performance issue in large Assembly

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Does it contain any assembly features like weld beams, chamfers?

 

Could you post a picture about assy (complexity)?

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Low performance issue in large Assembly

Phenom
Phenom
I would also check for broken links, also for textures.

I would make a copy of the assembly and all it's part on local drive and open it with the PC fisically disconnected from the network. If with this test the assembly start to fly there is a good possibility that there is broken links.

Re: Low performance issue in large Assembly

Legend
Legend
How do you check for textures... ?

Re: Low performance issue in large Assembly

Phenom
Phenom
Some years ago I had this problem and I have made a simple VB program to check them. I don't know if Revisiona Manager now find this broken links.

I can post my vb program if there is interest.

Re: Low performance issue in large Assembly

Legend
Legend
Would be nice to have that VB program.. will it detect the textures also ?

Reg.

Jan Bos