Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

MATCH PROPERTY SIMILAR TO AUTOCAD

Pioneer
Pioneer

IS THERE A SIMILAR BUTTON/KEY FOR MATCH PROPERTY AS IN AUTOCAD?  

4 REPLIES 4

Re: MATCH PROPERTY SIMILAR TO AUTOCAD

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
What kind of object are you trying to copy properties from/to?


Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: MATCH PROPERTY SIMILAR TO AUTOCAD

Pioneer
Pioneer
LIKE COPY PROPERTIES OF DIMENSIONS OR SKETCH IN DRAFT, SIMILAR TO AUTOCAD

In Solid Edge there is a command called Copy Attributes u...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In Solid Edge there is a command called Copy Attributes used to copy the prefix, suffix, superfix, subfix strings, dimension display type, or tolerance string from one dimension to another or the style properties associated with a dimension or annotation to another dimension or annotation

 

http://support.industrysoftware.automation.siemens.com/training/se/106/en_US/index.html#goto:dimensi...Smiley Tongue

 

There is no such command to copy element attributes to other elements that I'm aware of.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: In Solid Edge there is a command called Copy Attributes u...

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

A macro for Match Properties in Solid Edge is available at:

www.cadvertex.com

 

Tushar Suradkar

http://surfandcode.blogspot.in