Cancel
Showing results for 
Search instead for 
Did you mean: 

MIRRORING COPPER PARTS

Creator
Creator

First off, we are still on ST3 but will be updating to the latest ST here very soon.  However, I have not had success with this feature creation since the early days of SE.

 

Now for my question.  I have created some copper that will also have a mirrored version of it.  However, I have never been successful at the mirror feature in the assembly mode with copper.  I was talking with one of my co-workers recently about it and he just happened to go back to his desk and try the same thing on his computer.  He was successful at the same function that I was trying to do.  When I do the mirror steps, and the last step before "finishing", I see the copper mirrored.  However, when I hit the finish button, it pops up with the error:  "The part cannot be placed.  Make sure it is not a feature library part."

 

I compared his settings to mine and they are the same.

 

Anyone have any suggestions to this?

 

Thanks in advance!

2 REPLIES

Re: MIRRORING COPPER PARTS

Phenom
Phenom
Any screenshots there?

Re: MIRRORING COPPER PARTS

Valued Contributor
Valued Contributor

In my experience it will have to initialize the registry.
I occasionally initialize the registry if that happens.
Always have a registry backed up.