08-04-2015
05:09 PM
- last edited
Monday
by
AmyReyes
Hi Community,
ist es möglich das ih mit meiner Studenten Version die MPs downloaden kann?
Ich habe Windows 10 und ST7 und angeblich soll ST7 unter Windows 10 ab dem MP 4 und höher laufen!
Mit freundlichen Grüßen
Dennis
Solved! Go to Solution.
08-04-2015 07:16 PM - edited 08-04-2015 07:17 PM
Gyno wrote:Hi Community,
it is possible that IH can download the MPs with my student version?
I have Windows 10 and ST7 and allegedly ST7 10 run on Windows from the MP 4 and higher!
Yours sincerely
Dennis
Hi Dennis,
No.....the maintenance packs are only available to commecial users on "current" paid annual maintenance.
As yet Windows 10 is not supported, in any of the current [nor previous] versions of Solid Edge....although, some users [on commercial licenses] have done so, and reporting their success, it is not yet recommended to upgrade to Win10.
If Siemens were to update the existing application,....I suspect they would most likely replace the software package on their server, and users would then need to re-download it and the completely uninstall & reinstall Solid Edge.
[Also note: these are only my thoughts....I don't work for Siemens, and nothing official has been said to this effect]
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000
08-05-2015 05:33 PM
Hi there,
This thread might be of help to you..... >here<
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000
08-06-2015 04:33 PM
The Solid Edge ST8 Student Edition download is available now for you to download. It just posted within the past few minutes.
Please note that we are not aware of any serious problems running ST8 on Windows 10, but our testing is still underway and Solid Edge support running on Windows 10 has not been officially announced yet.
Please be sure that 3.5 .net (also required with ST7) remains installed on the machine.
Enjoy,
Laura
Solid Edge Release Manager
08-07-2015 11:41 AM
@LauraWatsonwo kann ich denn ST8 downloaden? Funktioniert das mit meiner Studenten Version?
Mit freundlichen Grüßen
Dennis
08-07-2015 12:27 PM
You can download the ST8 Student Edition here:
http://www.plm.automation.siemens.com/en_us/academic/resources/solid-edge/index.shtml
You will register and select the language of Solid Edge ST8 and receive a license key via email.
Laura
08-07-2015 12:34 PM
08-07-2015 02:01 PM