05-23-2017 10:29 AM
I accidentally selected multicolored sketch display for a sketch in my flat pattern, and now I can't get it to go back. The options for that sketch are now greyed out so I can't select single colored or uncheck multi color. This is very annoying because when I'm in another sketch and selecting elements from that sketch, I cannot tell the difference between the sketch i'm currently in or the sketch I activated this in. Then in a moment of brilliance I decided to activate this intentionally in another sketch, same result, cannot turn it off. Any ideas?
05-23-2017 10:46 AM
Hi @nominus38
Right Mouse Button and "Single Colore Sketch Display"
Does here exactly what it should!
05-23-2017 10:50 AM - edited 05-23-2017 10:53 AM
As I said, that option is greyed out and unavailable for this sketch. Don't know why, don't know how, but it will not let me select that.
05-23-2017 10:53 AM
Hi @nominus38
can You upload the file or show at least a screen shot from the complete Solid Edge window?
05-23-2017 10:54 AM
05-23-2017 10:59 AM
Hi @nominus38
for Your information:
is just the same here with a sketch in flat pattern mode.
Once changed to colored, no way back to single color!
Seems to be a bug!
05-23-2017 11:01 AM
Sorry I ruined your flat pattern.
05-23-2017 11:12 AM
this appears to be an IPA... I believe you can only toggle the sketch color with the part is open...
try to Open the part and see if you can then toggle the setting.
05-23-2017 11:14 AM
no, not IPA.
Just had a single PSM with flat pattern.
Exactly the same situation!
05-23-2017 11:15 AM
Tried. Does not work.