Cancel
Showing results for 
Search instead for 
Did you mean: 

MYSTERY BLOCKS APPEARING IN BLOCK SELECTION PANE

Not applicable

I keep finding blocks that I had once made and than deleted, I thought, showing up
in the BLP. I delete them and than the next time I open anther file, I find again.

I guess they must be somewhere in the SE programs files but I can't find them.
Thanks,
Ron
Ronald W Latour
2 REPLIES

Re: MYSTERY BLOCKS APPEARING IN BLOCK SELECTION PANE

Not applicable
Ron,
I'm not sure what you are saying. If you create a block in a file and then
delete the occurrence of the block, it will not delete the master block from
the file. It will only delete the occurrence. you have to go to the
ActiveDocument in EdgeBar and delete the block. This will remove all
occurrences from the file.
Regards,
Rick B.

Re: MYSTERY BLOCKS APPEARING IN BLOCK SELECTION PANE

Not applicable

Ricky, I didn't know that and now I think I understand what's happening. I created
a template file some time ago when I was playing with making blocks. I thought
that if I deleted the blocks from the Model environment, they were GONE.
I kept using the template file to start all of the new drawings that I'm currently
working on. So I went back and deleted the blocks from the template file.
Thanks,
Ron
"Ricky Black" wrote:
>Ron,
>I'm not sure what you are saying. If you create a block in a file and then
>
>delete the occurrence of the block, it will not delete the master block from
>
>the file. It will only delete the occurrence. you have to go to the
>ActiveDocument in EdgeBar and delete the block. This will remove all
>occurrences from the file.
>
>Regards,
>Rick B.
>
>

Ronald W Latour