Cancel
Showing results for 
Search instead for 
Did you mean: 

Macro/Add-in for automated creation of DIN471/DIN472/DIN7993/DIN6799 grooves

Genius
Genius

Does someone know a company that does have an addin or macro for creating DIN471/DIN472 /DIN7993/DIN6799 grooves

Dirk Rutten

Solid Edge STX user
2 REPLIES

Re: Macro/Add-in for automated creation of DIN471/DIN472/DIN7993/DIN6799 grooves

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

If your Solid Edge license has Standard Parts you can download from there.

 

Marc

Re: Macro/Add-in for automated creation of DIN471/DIN472/DIN7993/DIN6799 grooves

Genius
Genius

Hi Marc,

 

Indeed this is a solution if you don't want to do the complete proces of making a groove.

But I'm searching something where I only need to enter the shaftdiameter and the distance from and select shaft and reference plane.

I hate to say this but I'm missing this kind of automated feature creation in SE.

And yes it is possible to automate al this via feature lib but like most of us we don't have enough spare time to achieve a decend library. You know it's always I want to have it NOW.

Anyway thanks Marc

Dirk Rutten

Solid Edge STX user