Cancel
Showing results for 
Search instead for 
Did you mean: 

Major Excel Table issue ST9

I have a major issue with tables pasted into ST9.  Once I create a table in excel and paste it into the draft, im only able to double click and edit it ONCE.  after that, if I try to double click on it OR right click on it and open it in excel, a dialogue box pops up telling me that the object is NOT editable.

 

Capture.PNG

 

This will pose a HUGE issue as we have some pretty complex tables in our drawings.  Any ideas?  I am on MP7.

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments
2 REPLIES 2

Re: Major Excel Table issue ST9

Follow up.

 

If I shut down Solid Edge, I can edit it again.,,only once though

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: Major Excel Table issue ST9

Genius
Genius

Hello,

 

Do need to restart SE, try save document and this should help to the next close and open table. Had the same problem IR#8929009.

SE ST9 + TC 10.1.7