Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Make Two part dimensions the same

Experimenter
Experimenter

I was reviewing some old concept models my former counter parts created and ran into a part dimensioning technique I can not figure out.

Notice the 54.750 on the left and right. The left one is red so it can be modified. The right one is Blue and copies whatever I change the left one to.

How is this done?

I do not see any mirrioring or symmetricly releations going on.

 

Ken

Untitled.jpg

2 REPLIES 2

Re: Make Two part dimensions the same

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Ken,

There are several ways to do this but probably the most direct would be to double-click on the dimension that you want to be "driven" (blue) by the "driving" (red) dimension.  When you double-click on the dimension, you will get a menu at the top where you can rename, apply a formula, comment, etc.  Click on the value of the "driving" dimension and it will make them equal..

If you go to Tools-Variables, you'll get more details on "stuff" you can do with all the variables in your model.

Equal Dims.JPG

 

Hope this helps,

Kevin

 

Kevin Grayson
Solid Edge Technical Consultant
kevin.grayson@siemens.com

Re: Make Two part dimensions the same

Phenom
Phenom

I do this trough the variable table most of the time.

There you can add a lot like this:

VariableTable.png

You see the variable "as"? That's made in the table. Other dimensions are calculated from this one.

You can even use them in other files:

VariableTable2.png

 

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user