Cancel
Showing results for 
Search instead for 
Did you mean: 

Make part show up in draft

Honored Contributor
Honored Contributor

Attached is a part file. This was imported from a pera-solid file.

 

What do I need to do to make all of the 3 sub parts show up in the draft environment?

 

 

eidt------

 

I think the key problem is that the model is surface only. What's the key term to look up in help or whats the command to take enclosed surfaces and turn into a solid.....IE the solidify command?

 

I stay away from surface modelin and try to stay in sheet metal. This is my first time trying to turn surfaces into solids.

 

 

4 REPLIES 4
Highlighted

Re: Make part show up in draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Show surface bodies in the views.

surfbods.JPG

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Make part show up in draft

Honored Contributor
Honored Contributor

Thank you,

 

That allowed me to find my stumbling block. I needed to to display all under the part in draft so that I could see and turn the surface on.

Re: Make part show up in draft

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also....have you tried opening that file into an Assembly template, to see if they come in as solids?....as the component looks to be modelled as it would be made, in 2 components + the o-ring.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Make part show up in draft

Honored Contributor
Honored Contributor

I have, that didn't separate the parts. Originally the file was Solid works single part.