Cancel
Showing results for 
Search instead for 
Did you mean: 

Make the command bar vertical?

Valued Contributor
Valued Contributor

Ive set in the settings to make the command bar vertical but it still shows it like this??

 

Capture.PNG

Regards,

MagRiz
(ST9 User Est 01.18)
13 REPLIES

Betreff: Make the command bar vertical?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

the form You are showing is not the Command Bar but the relation value bar

 

If set to Vertical You will see the Command Bar as following:

 

20180223_1327.PNG

regards
Wolfgang

Betreff: Make the command bar vertical?

Valued Contributor
Valued Contributor

Thanks, how do i get the relation value bar to be vertical. On another machine with SE i use it is vertical 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Make the command bar vertical?

Siemens Phenom Siemens Phenom
Siemens Phenom

I'm not sure what you saw, but there is no way to make the relationship value bar vertical - it is always horizontal.

 

Greg

Betreff: Make the command bar vertical?

Valued Contributor
Valued Contributor

ill update this thread later when im on my other machine

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Make the command bar vertical?

Valued Contributor
Valued Contributor

Hi,

Sorry for the late update and confusion in OP as what i meant was, when i DOUBLE click the mate i dont get the vertical bar NOT when i click it ONCE as i made out to be in the OP.

 

but this is what i mean, when i click on a mate in the tree once i get this

Capture.PNG

 

when i click on edit definition i get this

 

Capture 2.PNGon my other machine i wasn't getting this vertical bar and was wondering how to sort it out.

 

what i might do for future is save out my settings from this machine and load them on other machines i work on.

 

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Make the command bar vertical?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

 

depending on Your settings in SE Options You either can have horizontal or vertical toolbars

 

If set to vertical 

20180226_1235.PNG

 

 

it looks like that

 

20180226_1236.PNG

 

otherwise it is the small horizontal toolbar

 

regards
Wolfgang

Betreff: Make the command bar vertical?

Valued Contributor
Valued Contributor

@hawcad

Thanks, ill try that out.

 

by the way, how do i save the settings from options panel to export them out . 

I only see a save option in another settings panel, which is in Customize

Regards,

MagRiz
(ST9 User Est 01.18)

Betreff: Make the command bar vertical?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You could save it as a theme (which is saved in "customization") and distribute that to all workstations. But that will momentarily override any existing custom themes. So I would think it's not worth it unless your user count is very high and no users customize their menus. Unless someone knows a registry tweak. Just change the options on all the machines.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Betreff: Make the command bar vertical?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

the vertical tool bar is an option if You are using the theme "Maximum Assistance"

 

You can use this evrywhere or create Your own theme and copy this theme from one machine to another.

I would not change the default themes, always create Your own.

 

regards
Wolfgang