05-21-2014 02:46 PM - edited 05-21-2014 02:51 PM
NEVER MIND... found the tool in the SE Viewer & Markup program
=================
We recently made some network changes, and the server name that all the SE files are on got changed (from "xxx-appl" to "xxx-app01"). No changes to the directory structures or anything, just the server's name.
Is there a tool to do a mass replace/update of every link?
(i.e. change every instance of "\\xxx-ati-appl\" to "\\xxx-ati-app01\" in the links of every .par, .asm, .dft, .cfg, etc...)
07-03-2014 09:30 AM
Same. This is a HUGE problem with linked files.
How was this "SOLVED" ?
07-03-2014 12:28 PM - edited 07-03-2014 12:29 PM
There is a button in View and Markup utility called "Redefine Links", under the Tool tab. Attached is a screenshot of the important part of the utility, in which you type in the section of the current link path you want to replace, and what you want to define the new link path is. This will crawl through all Solid Edge files in the folder you select, and replace that section of the link.
I had to do a server base name change earlier this year and was quite worried about it, but it ended up being almost painless. Good luck.