Cancel
Showing results for 
Search instead for 
Did you mean: 

Me ajudem com license Solid Edge Student

N/A

Já fiz tudo que pude...reinstalei como administrador , renomei o arquivo de licença mais sempre aparecea a mensagem : The feature solidedgecademic failed to check out for the following reason:
System clock has been set back,
Feature: solidedgeacademic
License path: C:\ Arquivo de programas\solid edge st4\program\SELicense.dat;
Flexnet Licensing error: -88,309
For further information, refer to the FLEXnet Licensing documentation,
available at"www.flexerasoftware.com"
....e mais alguma coisa depois

2 REPLIES

Re: Me ajudem com license Solid Edge Student

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Olá,

Pesquisei na base de dados da Siemens, e o que encontrei foi isto:

SYMPTOM/PROBLEM
---------------
Solid Edge issues the following message:

System clock has been set back.
Flexlm error -88,309

SOLUTION/WORKAROUND
-------------------
This message occurs when the user is using a temporary or dated license file
and sets the system clock back to a date prior to license expiration.

FLEXlm checks the dates of certain files and if it finds files that
have dates into the future, the license key will not work and will prompt an
error.

Your only choice is to rebuild the machine. Rebuilding the machine (complete
rebuild) and setting the clock correctly will resolve the error.


Agora, eu não percebo o que querem dizer com "Rebuild the machine".

Can someone from Siemens help this user about what it means to "rebuild the machine"?

Re: Me ajudem com license Solid Edge Student

N/A
Carlos, this means reinstalling the OS.
The only other option when running into these FlexLM problems is to use
a non-timestamped license file (permanent). And that normally is a
regular purchased license.
Regards, Ulf
Ulf Eriksson
Siemens Industry Software
GTAC EMEA Support - Nordic
On 2012-04-27 10:40, edocf014 wrote:

>
> Can someone from Siemens help this user about what it means to "rebuild
> the machine"?
>
>