Cancel
Showing results for 
Search instead for 
Did you mean: 

Measure minimum and maximum thickness of a part

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

 

Someone knows if there is an application implemented in a command or button so that when it runs show the minimum and maximum thickness of the part and the location of each one.

2 REPLIES 2

Betreff: Measure minimum and maximum thickness of a part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @xeniaturon

 

 

 

the only way I can imagine to get this result might be to have a a part with two bodiesin it.

The inner body and the outer body

 

Then You can measure the minimum distance between those two bodies

 

20170904_1754.PNG

 

Of course You can change the option to show the maximum distance, but this nwo will not be a perpendicular distance bewtween two surfaces

 

20170904_1755.PNG

 

So to find the maximum thickness is not that easy and needs a more induitive method by the user

 

 

regards
Wolfgang

Re: Measure minimum and maximum thickness of a part

Siemens Phenom Siemens Phenom
Siemens Phenom

As far as I know, there is no explicit application to find this.

 

One workaround might be to use SE Simulation to apply a pressure to e.g the inside of the model, then plot the displacement or stress. The model then doesn't need to be water tight.

 

To measure the detailed thin wall section then place a Cross section and place Measurements.  

wallthickness.jpg

 

 

Good luck!

 

/Ulf

Siemens EMEA GTAC Support