Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Measurement of a 3D sketch

Valued Contributor
Valued Contributor

Hello my friends,

I created a model for design copper pipes for my work, I mostly use a 3D sketch to design them and I need to obtain the total lengh of the 3D sketch.

I use the measure command and then I click to the command "create a variable" to expose it for use on the draft, but I always have to do it by hand, is it possible to do it automatically, for example assign a variable that grow it's value while I build the 3D sketch?

 

TIA for answering

5 REPLIES 5

Betreff: Measurement of a 3D sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Davide_Parolin

 

 

 

may I ask You which license type You have?

 

Do have xPres Route too?

 

 

regards
Wolfgang

Betreff: Measurement of a 3D sketch

Valued Contributor
Valued Contributor

Hi @hawcad,

No I don't have Xpress route licence, I always do them easily using the sketch 3D, so I don't need that icence... 

Betreff: Measurement of a 3D sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Davide_Parolin

 

 

 

no need for a xPresRoute license.

 

You just can use the Structure Frame feature in assembly.

Create Your pipe using a Frame component and You will get the Straight Length in draft BOM automatically

 

20180802_1654.png20180802_1656.png

 

And another advantage here is, that You can draw Your 3D sketch with simple lines only. No need for arcs.

This will be a value within the Structure Frame option settings.

 

regards
Wolfgang

Betreff: Measurement of a 3D sketch

Valued Contributor
Valued Contributor

Thanks @hawcad, this is a very easy and functional solution!

 

 

Betreff: Measurement of a 3D sketch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Davide_Parolin

 

 

 

welcome, happy to hear that!

 

 

regards
Wolfgang