Cancel
Showing results for 
Search instead for 
Did you mean: 

Measuring between entities

Creator
Creator

Hello,

 

I am trying to get a measurement between the X-Y plane and a face on a body but when I put the x-y refplane as element 1 and the face of the body as element 2 I get no results.

 

When I manually do the command (measure minimum distance) I get the result I am looking for.

 

Any help would be nice.

 

Thanks

 

 

5 REPLIES 5

Re: Measuring between entities

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hello @TS-GSSO

 

Do you mean a call to the Meaurement API function call ?

In that case, the Solid Edge Developer Forum is the recommended place to post this for a better response.

 

Tushar

www.SurfAndCode.in

Re: Measuring between entities

Genius
Genius
have you tried using the "measure" command under the Inspect, 3D measure. Select your plane and face. then change "distance type" to min.
Cory M
Solid Edge ST10
ST10 Cert

Re: Measuring between entities

Honored Contributor
Honored Contributor

Most of the time, I find it faster to create a new sketch to get the needed measurement. The mixture of edge types can be isolated this way using includes and sketched lines.

Re: Measuring between entities

Gears Phenom Gears Phenom
Gears Phenom

I tend to just use PMI for this, as that way I never have to go back and check what that measurement is again. As I've gotten older my brain seems to forget things I just looked into. BTW what time is it again?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"

Re: Measuring between entities

Phenom
Phenom

I always use measure minimum distance and just change the element location type as I need.

HP Z420 16GB RAM
Quadro K4000
ST10 MP12 on Windows 10 Pro 64.