Cancel
Showing results for 
Search instead for 
Did you mean: 

Memory Usage High

Creator
Creator

Need a little insight from other SE user. Have any of you experienced SE using a large amount of memory? 

I am working on an injected molded part with a normal number of rounds for a molded part and my memory usage seems extremly high which i beleive is the cause of SE processing very slowly when applying round. I thank you in advance for any insight or suggestions you can provide. 

5 REPLIES 5

Betreff: Memory Usage High

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

HI @SColler

 

 

which Solid Edge version are You using?

 

And if talking about high memory, is it possible to show the performance pciture from task manager?

 

 

regards
Wolfgang

Betreff: Memory Usage High

Creator
Creator

ST9 MP6

I have noticed this issue with ST8 also. 

Betreff: Memory Usage High

Gears Phenom Gears Phenom
Gears Phenom

I have noticed a big increment in memory usage with ST9 compared to ST8.

 

It seem that it doesn't release memory when closing files.

 

It could be one reason of the ST9 slow down

Highlighted

Betreff: Memory Usage High

Creator
Creator

I have noticed that it holds the memory until SE is closed down, thus causing SE to run slow. 

Betreff: Memory Usage High

Honored Contributor
Honored Contributor

I reboot twice a day, more if the vid card runs out of memory (SE/Nvidia/W10 has vid memory leaks). And if the vid card does not have 4GB or more, then that load gets put on the ram/CPU.