Showing results for 
Search instead for 
Did you mean: 

Memory Usage

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Edgers,

we have seen a "strange" behaviour of Solid Edge ST6 MP9 (but not only MP9) that when opening a Solid Edge document (not depending what type of document) an close it (with or without save) the memory consuming of the Solid Edge task increase by 5 to 10 MB.


This sounds not that much, but when having a batch job running, with opening and updating 100s or 1000s of SE documents, then it seems, that an memory depenging error will occur (or task depenging or whatever).


The result is a memory consuming of SE of up to 1 GB or more

even there is nothing opend by SE.


Has anybody seen the same or was anybody running into same problems?


Thanks and regards