Cancel
Showing results for 
Search instead for 
Did you mean: 

Menu auto hides when i go into a command

This is hard to explain, i will post a picture, but my menu tabs have decided to disappear when I go into a command. Is there a way to "repin" them down?

Capture.JPG

4 REPLIES

Re: Menu auto hides when i go into a command

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

This appears to be a graphcis/card related issue.

If you just hover the mouse over the ribbon, does it show any tooltips or able to start a command by clicking blindly ?

 

What is the OS used, the RAM and the graphics card driver version ?

 

Re: Menu auto hides when i go into a command

Sorry, I thought I had email notifications turned on, I did not. I went home for the weekend and came back this week and it fixed itself. I do not remeber if hovering brought the tooltips up or not.

 

 It is interesting that you say it is a graphics related issue. I am now having other issues with dimensions displaying correctly that I have addressed in a new thread.

 

 

BTW, i am using windows 7, intel i7-2600 @ 3.4Ghz 4Gb ram 

Re: Menu auto hides when i go into a command

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Wow, awsome configuration ! - no doubt it self-corrected the issue while you were away on a weekend Smiley Happy

 

Re: Menu auto hides when i go into a command

Yes, we paid extra for that add onSmiley Wink