Cancel
Showing results for 
Search instead for 
Did you mean: 

Merger from previous forum - SE SP forum gone?

Creator
Creator

Hi,

 

After the merge to the new forums, I can't seem to locate the forums for Solid Edge SP.

Does anyone know where I can find them?

 

Thanks.

3 REPLIES

Re: Merger from previous forum - SE SP forum gone?

Community Manager Community Manager
Community Manager

With the old BBS setup, 98% of stuff went into Solid Edge Misc. So in the new setup, there is just one place to put everything. Please post SESP questions here, along with the rest of SE. Any topic area that get's big enough, we may separate out, but so far so good with a single area for everything. 

Dan Staples
Director, Solid Edge Product Development

Re: Merger from previous forum - SE SP forum gone?

Creator
Creator
Well the old forums had more than 100 posts regarding SP, so I guess those were deleted.

Anyway I'll post here then, thanks!

Re: Merger from previous forum - SE SP forum gone?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi there,

Only maintenance customers can see them (therefore, have access to) the archive of the old (now read only) BBS forum posts, including SE-SP, but they are there still.
>> http://community.plm.automation.siemens.com/t5/Solid-Edge-SP/bd-p/Customer-SolidEdge-SP <<
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019